Testa att söka på nyckelord, orderkod eller produktkod, eller serienummer t.ex. ”CM442” eller ”teknisk information”
Enter at least 2 characters to start the search.
  • Historik

Speed and accuracy help to meet stringent quality demands

QuickSens technology improves Ultra High Temperature (UHT) process at Chr. Hansen in Denmark

By switching to the iTHERM TM411 temperature sensor, the Danish site successfully improved the temperature monitoring, which is critical to the UHT treatment of the nutrient solution. Furthermore, the process remains closed during recalibration.

Calibration of temperature sensor in a laboratory by Tommy Mikkelsen, metrologist at chr Hansen Chr Hansen

The results

  • Plant availability is increased.

  • The temperature sensor enables higher process safety

  • No additional CIP cleaning procedure is required after a recalibration

  • The solution contributes to the reduction of the maintenance costs

Calibration of temperature sensor in a laboratory by Tommy Mikkelsen, metrologist at chr Hansen

"The new iTHERM TM411 thermometer with QuickSens technology is the perfect choice for this application. Furthermore you don’t need to stop the process during calibration."

Tommy Mikkelsen, Metrologist
Chr. Hansen

The challenge

Both, very accurate temperature control and very fast response to temperature changes are vital for the efficient and safe production of bacterial cultures, which are used for sour milk products such as yoghurt and other types of food. During the UHT (Ultra High Temperature) treatment, the temperature must be kept above 139˚C (282°F) otherwise in the worst-case scenario, the production batch might have to be destroyed.

Our solution

Tommy Mikkelsen conducted extensive testing of the iTHERM TM411 temperature sensor with convincing results. Its unmatched response time allows continuous process monitoring and enables a constant temperature to be maintained within a very small range. The tests also showed that the predictable negative impact of the thermowell on the overall accuracy was hardly detectable. Thus the recalibration required for this critical device can be performed without interrupting the process.

Safe sterilization required

In the UHT process, a medium is being exposed to temperatures above 139°C (282°F) for a defined time span. Safe sterilization can only be guaranteed if the temperature does not fall below the minimum temperature at any time. Thus, if the temperature drops and comes close to the minimum required temperature, a quick response from the control system is necessary to counteract the temperature decrease. The prerequisite for this reaction is a temperature sensor with a very fast response time.

©Endress+Hauser

Unmatched response time for quality improvement

Tommy Mikkelsen has conducted response time tests with different temperature sensors which revealed that iTHERM QuickSens technology could reduce response times by more than 50% compared to older sensors! “The new iTHERM TM411 thermometer from Endress+Hauser with QuickSens technology is the perfect choice for this application”, says Tommy Mikkelsen. “ Its unmatched response time allows continuous monitoring of the process and keeping the temperature constant within a very small range.”

The negligible impact of the thermowell

A thermowell is the part of the thermometer which hosts the actual sensor (or insert) and protects it from harsh process conditions. This additional barrier between the sensor and the process medium usually negatively affects the performance of the meter. To quantify this expected negative impact on measurement performance, Tommy Mikkelsen has conducted test calibrations both with and without thermowell: measured deviations are below 0.1˚C – regardless of whether there was a thermowell or not!

A thermowell sealed inside a food and beverage hygienic process ©Endress+Hauser

Recalibration made easy

Using thermowells offers a significant advantage: during recalibration the process can be kept closed as the thermowell remains in the plant while the sensor itself is removed for calibration. Removing the sensor for recalibration is child’s play: the so-called QuickNeck allows the tool-free removal of the complete upper part of the sensor from the thermowell with just one twist. No need to open the housing or to disconnect any wires – it is simple, safe and fast.

©Endress+Hauser
  • Enkla produkter

  • Enkla att välja, installera och använda

Tekniska egenskaper

Enkelhet

  • Standardprodukter

  • Pålitliga, robusta och lätta att underhålla

Tekniska egenskaper

Enkelhet

  • High-end produkter

  • Mycket funktionella och praktiska

Tekniska egenskaper

Enkelhet

  • Specialprodukter

  • Designade för krävande applikationer

Tekniska egenskaper

Enkelhet

Varierande

FLEX urvalet Tekniska egenskaper Enkelhet
  • F
  • L
  • E
  • X

Fundamental urvalet

Möt dina grundläggande mätbehov

Tekniska egenskaper
Enkelhet
  • F
  • L
  • E
  • X

Lean urvalet

Hantera dina kärnprocesser med enkelhet

Tekniska egenskaper
Enkelhet
  • F
  • L
  • E
  • X

Extended urvalet

Optimera dina processer med innovativa teknologier

Tekniska egenskaper
Enkelhet
  • F
  • L
  • E
  • X

Xpert urvalet

Hantera dina mest utmanande applikationer

Tekniska egenskaper
Enkelhet

Varierande