Testa att söka på nyckelord, orderkod eller produktkod, eller serienummer t.ex. ”CM442” eller ”teknisk information”
Enter at least 2 characters to start the search.
  • Historik

Focused on the future

Expansion and modernization of the Basel wastewater treatment plant

The Basel wastewater treatment facility (ARA) has been in operation since 1982. After 40 years, the plant is reaching its limits in terms of age and capacity. In addition, the requirements and stipulations outlined in the water protection act have changed significantly with respect to microcontaminants. As operator of the ARA Basel, ProRheno AG aims to meet these future requirements with the expansion and modernization of the facility.

Wastewater treatment plant ARA Basel, view over the SBR ©Endress+Hauser

View of the SBR at the ARA Basel wastewater treatment plant.

Industry experts in discussion ©Endress+Hauser

Industry experts in discussion: Joscha Giambonini, HOLINGER AG (left) and Marc Bircher, Endress+Hauser (right).

View of the SBR at the ARA Basel wastewater treatment plant.

Customer benefits

  • Reliable adherence to current regulatory threshold values

  • Ease-of-implementation in response to strengthening of the water protection act, thus eliminating the need for new modifications

  • Improved environmental and water protection

  • Increased sustainability

Project leader ProRheno AG

“Many factors contributed to the decision to select Endress+Hauser, including openness, regional proximity and reliability. Collaboration with the staff is excellent.”

Roberto Frei, Project Manager
ProRheno AG, Switzerland

Customer challenge

ProRheno AG decided as early as 2008 to retrofit the ARA Basel municipal treatment plant. From the beginning the plan was to implement the project without interrupting the operation of the plant. Large-scale projects like these call for forward-looking planning and the right partners.

Project realization

The tender offer for the project stipulated that the instrumentation supplier also cover installation, commissioning, training and documentation. As a complete provider, Endress+Hauser fulfills these requirements and offers a solid foundation for successful collaboration.