Testa att söka på nyckelord, orderkod eller produktkod, eller serienummer t.ex. ”CM442” eller ”teknisk information”
Enter at least 2 characters to start the search.

Optimized cleaning for maximum product quality

thyssenkrupp measures cleaner concentrations with Teqwave I

Teqwave I from Endress+Hauser provides thyssenkrupp Presta AG with a new reliable solution for monitoring cleaning media in its spray and flood part cleaning machines. Teqwave uses special sound waves to create an acoustic “fingerprint” of the high-quality cleaning media being used. This enables Teqwave to detect their concentration in cleaning baths continuously and with high precision.

part cleaning machine at thyssenkrupp Presta AG Copyright by thyssenkrupp Presta AG

Part cleaning machine at thyssenkrupp. The concentration of the cleaning medium is measured using the built-in Teqwave I.

part cleaning machine with built-in Teqwave I Copyright by thyssenkrupp Presta AG

Part cleaning machine at thyssenkrupp. The concentration of the cleaning medium is measured using the built-in Teqwave I.

The result

  • Safeguarded process quality thanks to real-time measurement with high accuracy

  • Quick reaction through immediate readjustment in case of changes in the cleaner concentration

  • Minimum risk of errors, for example, as caused by writing down measured concentration values by hand

picture of Mario Hörler, Project leader at thyssenkrupp Presta AG

Endress+Hauser has totally convinced me with the function, performance and technical design of this high-precision solution.

Roman Nägele, Technical Project Leader
ToolingCompetenceCenter, thyssenkrupp Presta AG, Oberegg (Switzerland)

The challenge

The concentration of the cleaning medium used to be measured once a week by a specialist using an elaborate titration method. This process included documenting the measured concentration values, which are crucial in maintaining the desired process stability. Both the measurements and the documentation were very time-consuming and made intensive use of consumables. In addition, the process of reading out measured values manually during titration and documenting them proved to be very error prone.

Our solution

With the installation of